Other Parts Discussed in Thread: TPS2HB16-Q1, TPS22990, TPS22959
Hi team,
we have urgent support needs below.
My customer has a new requirement below.
3.3V input, dual channel current limit port protection ( 5A per channel) device.
MPS has promoted the MP5092 to them. We only can promote the TPS22976 to them.
But we still have below questions want to check with you.
1. What's the difference between the load switch and efuse?
2. TPS22976 max current is 6A, whether the device has current limit feature internal the device? if yes, what''s the current limit threshold?
3.If the customer need current foldback Ios feature to improve the short circuit protection, do we have some recommended devices?
4.We need the device has current limit feature( current limit threshold setting feature is optional). Do you have some recommended devices?
Many thanks.