Hi,
I am considering using the TPS4H000-Q1 device.
I would like to ask you about the current limiting feature of this device.
Set R(CL) of CL pin to 2.4kΩ to set the current limit to 100mA.
I think that it is good to do.
From the formula (4) on page 17 of the data sheet, it can be calculated as follows, considering the Typ value.
R(CL)=[Vcl(th)×K(CL)]/Iout
=[0.8(V)×300]/0.1(A)
= 2400 (Ω)
=2.4 (kΩ)
External current limit accuracy is ±20% because it corresponds to I(limit) ≥ 100 mA.
What I would like to ask is the following description on page 7 of the datasheet.
Does this mean a 150mA overload is required to detect at 100mA current limit?
If the current slowly approaches 100mA, does that mean there is no limit at 100mA?
*Notes on page 7 of the data sheet
(2) External current limit accuracy is only applicable to overload conditions greater than 1.5 x the current limit setting
Best regards,