Other Parts Discussed in Thread: TINA-TI,
Hi,
I have built a bunch of boards with this regulator for a 5V output. Most of them work okay. Some failed, outputting either ~0.6V or ~1.3V.
Vin = 9V to 13V, En = 5V, L=2.2uH, Cin = 10uF, Cout = 22uF + 4.7uF
I took a scope shot of a bad regulator, and it seems to have a short spike once enable pin is turned on, but goes back to 0V, and gradually rises(like an RC charging waveform) to 1.3V. One channel is on the IC switch output, the other channel is after the inductor, on the node where it should have been 5V. I checked the inductor with an LCR meter and it is indeed 2.2uH. What could have caused the IC to be damaged?
Thanks,
Enyu