Dear Sir,
when Vac input is 264Vac. it happened cross over wave between GDA and GDB.
It is correct?
Z1: GDA
Z2: GDB
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
when Vac input is 264Vac. it happened cross over wave between GDA and GDB.
It is correct?
Z1: GDA
Z2: GDB
Hello Dexter,
Thank you for your interest in the UCC28064A Interleaved PFC controller.
The waveforms shown at Z1 and Z2 are the Vds of the two switching MOSFETs, not GDA and GDB.
However, the phase relationship of these waveforms is correct, and therefore GDA and GDB are correct by inference.
Regards,
Ulrich