Other Parts Discussed in Thread: BQ24090, , TPS2511, TPS61032
A view days ago, i was designing a small powerbank with integrated lipo charging ic. I want to charge mobile Phones, Headphones and so on. I used the BQ24090 and it works fine. For the step up switch I used the TPS61030 and for charging smartphones I used the TPS2511. After designing and soldering I was testing the circuit but I can't find the Problem. If I put my mobile Phone on it, it starts charing for one second and stops after this one second. When I measure the voltage, I measure 4.98V without any load. With Load there are 4.68V, but it doesn't work anyway. The charging of the battery works fine. I put the schematic to this post. I hope you can help me.
Thank you
best regards
Julian