Hello,E2E TI Expert ;
I am now using your CRM PFC controller UCC28056, and I am now with some problems with the controller;
1) The DC output voltage rises with the increase of the input AC power voltage, and it is difficult to maintain the desired set value of 400VDC; My test data are as follows:
Vinac_RMS(V) |
Iinac_RMS(A) |
Vout(VDC) |
Rload(Ω) |
Pout(W) |
η |
85 |
0.677 |
211 |
820 |
54.3 |
94.4% |
90 |
0.696 |
220 |
820 |
59.0 |
94.2% |
100 |
0.63 |
222 |
820 |
60.1 |
95.4% |
110 |
0.669 |
239 |
820 |
69.7 |
94.7% |
120 |
0.696 |
254 |
820 |
78.7 |
94.2% |
150 |
0.667 |
277 |
820 |
93.6 |
93.5% |
180 |
0.701 |
310 |
820 |
117.2 |
92.9% |
200 |
0.681 |
322 |
820 |
126.4 |
92.8% |
210 |
0.687 |
332 |
820 |
134.4 |
93.2% |
220 |
0.688 |
340 |
820 |
141.0 |
93.1% |
230 |
0.676 |
344 |
820 |
144.3 |
92.8% |
240 |
0.686 |
349 |
820 |
148.5 |
90.2% |
Note:Desired Vout voltage :400VDC. |
2) It seems that in all working states, the circuit is always in CRM working mode, even though the load is small, the circuit is still not in DCM working state.