Hello,
if the input voltage of the BQ24703PW is above 23 volts (with no battery) the IC shuts down the transistor at the ACDRV pin. Why?
The resistor between GND and ACDET is 7k5 and the against input voltage is 100k. So it should start at around 18V.