Hallo,
I have made a designed base on a daisy chain of 15 TLC5940.
The project is working since about 1 years whitout problem. But today when I power on the board, it happens that one LED was on and the remainder was off which has never happened.
I keep on wondering what could be the cause. i made all the measurement on all the input signal the look quite ok.
The LED is power with 5V and connected to the TLC5940 which is power with 3,7V. Could this be the problem??
When power the TLC5940 with 3,7V, what is supposed to be the output voltage of the OUT0-OUT15, when the driver if off? Because I am measuring different voltage on different pin ranging fromm 2,65V to 3,7V on the same TLC5940