Ulrich
Is there any problem if the exposed pad meant for thermal reasons is not soldered to the pcb pad in this prototype phase?
Our last attempt(Friday) to get NTC pin to be as in the Eval board had the controller fail quickly.
Our sense is that it was due to excessive heat during attempts to solder the exposed pad. We cannot reflow it with all the parts in place. So we used hot air - thermocouple in vicinity showed controlled hot air temp to be 230 deg C. But it lasted several minutes & still did not flow the solder. Heating it further did it.
Then of course we had to hand solder the pads also at high temp.
When power up to 20 V or so...it quickly failed.
We are going to reinstall now. With conductive epoxy dot at the center just to have easy alignment of the chip to pads. & Will solder at leat temp recommended for good solder flow.
- Also: seems NTC pin may not be used for EN/disbale by an Opto . I am suspecting the plastic pkg if transparent & the phototransistor is conducting ...( I have experimental verification of this in a previous life ..& vendor had to change the material!)....of course I cannot be sure of this: why NTC pin will tend to be low...just before the controller failed Friday.
-so removing the Opto from NTC pin from now on.
robin