My problem is voltage drop out.
I'm using two LM5141 - 1 for 3.3V, 1 for 5V.
5V buck is okay, but 3.3V buck has a problem sometimes.
PWR_12V is a power source from adapter or power supply.
When I set voltage to 9V, 10V or 14V, it has no problem,
But when I use 12V, it occurs with over 50%.