Other Parts Discussed in Thread: TLV274, LM3409
Hi Irwin,
I have a quick question with regards to the Iadj pin of the LM3409HV. When the IC is disabled (EN=0) I measure 400mV on the Iadj pin, but when I enable it (EN=1) the measurement jumps to just over 800mV.
The voltage is supplied from the output of a TLV274 OP AMP (voltage follower) with an RC circuit (1K + 0.1uF) as in the EVM. I presume that this may be somehow related to the 5uA bias current on Iadj, but I can't see how the voltage measured on the Iadj pin would almost double when the driver is enabled.
Any thoughts?
Regards,