Other Parts Discussed in Thread: TPS7A24, TPS7A20, TPS7B69, LP2985, TPS784, TPS784-Q1
Hi expert,
TPS7A05 was mass production on customer side. Now there is a new project need LDO. Here is the requirement, could you recommend a new device for us ?Thanks.
Input voltage range: < 8V
Output voltage: Fixed to 5V
Max output current: 100mA
Start-up sequence: Less than 800us
Package: Better for SOT23-5, other package is also fine (Better p2p of TPS7A05--SOT23-5 pacakage)
Feather: Cost sensitive
Best Regards
Songzhen Guo