Dear Specialists,
My customer is considering TPS23754 and has a question.
I would be grateful if you could advise.
---
I have one question regarding TPS23754.
It is necessary to have a specification that informs the internal software whether the external power supply or PoE + is supplied by TP23754.
So I wondered if the T2P terminal could be used, but the enable conditions for T2P are as follows.
(VAPD> 1.5 V) OR (1.55 V< VPPD< 8.3 V) OR (type 2 hardware classification observed)
When supplying power by either external power supply or PoE +
Either way, T2P will be active.
Is it possible to output some kind of detection signal only when the TPS23754 is supplied with external power?
Or is it necessary to add a detection circuit externally?
---
I appreciate your great help in advance.
Best regards,
Shinichi