Other Parts Discussed in Thread: TPS2663
I am trying to use the LM5069 for a design that I have which has a very large hold up capacitor on the output of the LM5069. (64mF). The application would like to keep the inrush current to under 20A. I've tried to complete the calculator spreadsheet with my design parameters but there are a few output cells that are staying red saying that the slew rate generated will not keep the MOSFET in it's SOA. I am looking for assistance to determine the issue and finding a solution to this problem. I've attached the calculator excel sheet for reference.LM5069_Design_Calculator_REV_C1.xlsx