Part Number: LM25145
Other Parts Discussed in Thread: CSD18543Q3A, LM5146-Q1, LM61460
Good morning,
I used the quick calculator and webench tool and did my design.
Do you think should I add an RC snubber, gate resistors, and a Rbst in series with Cbst(Cbst is already in the design) by default or maybe not all but some of them?
Input Voltage 24V Output Voltage 5.1V, 534 kHz Switching frequency, 47N SS capacitor(4ms), CSD18543Q3A is used for both mosfets (60V-35A). Continuous current 4.4A
I am really limited with the layout space at this moment but I also dont want to take a risk. If you suggest me to add any of the an RC snubber, gate resistors, and a Rbst in series with Cbst.
If you need any other info please let me know.
Best Regards
Onur