Hi Team,
Here is a question on LM74700-Q1.
In datasheet 10.1.1.4, it recommend using two uni-directional TVS diodes to protect from positive and negative transient voltages. And in Figure 10-3, it recommend using SMBJ58A. But this part has 64.4V-71.2V Vbr , and LM74700-Q1 has 65V abs max input voltage spec, so it seems the margin using SMBJ58A is not enough. Please kindly add your comments why we recommend that TVS part, is it because the 65V spec for LM74700-Q1 has margin ? Thanks.
BRs
Given