Normal 0 false false false EN-US X-NONE X-NONE MicrosoftInternetExplorer4
Hi everyone,
We found that ~50% of boards showed significant noise on a 3.3V supply. The signature of the noise had a consistent frequency of ~400kHz but the amplitude varied from board to board.
I have included a portion of our schematic. We have confirmed that the noise is still present on the board even when we have stripped it down to just the power supply and PIC circuitry - removed Ethernet, op-amps, and wireless circuitry (present on the rest of the schematic).
The product uses an off the shelf 5V DC regulated supply. Further experimentation, using a variable output bench top power supply, showed that the amplitude of the noise changed as the input voltage decreased/increased. It seems that once the input voltage exceeded 5.1V the noise went away – although this varied from board to board that I tested. In some cases the noise didn’t go away until the input voltage exceeded 6V.
The problem has been resolved by swapping the 3.3V LDO (TLV1117) with one from Diodes Inc (ZLDO1117). Using the ZLDO1117 shows no noise on the 3.3V output.
Any ideas???