This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23753 circuit part alternatives

Other Parts Discussed in Thread: TPS23753, CSD17527Q5A

Hi All

I'm using TPS23753 in the same configuration as seen in the TPS23753AEVM-235 circuit.

[http://www.ti.com/lit/ug/slvua27a/slvua27a.pdf]

However i'm not using the diode rectifier shown in the schematic, I'm using MB4S bridge rectifier. Rest of the circuit is the same.

For the transformer, I'm using Wurth 749119350 [katalog.we-online.de/.../749119350.pdf] instead of Coilcraft NA6223-AL with changes to pinout as shown below

Coilcraft

Wurth

3

5

4

6

1

3

2

1

10

10,11

7

9,8,12

6

7

For the output mosfet, i'm using BSC057N08NS3 instead of CSD17527Q5A.

Above alternatives have been proven to work and produce stable 5V.

I would like to know if there are any alternatives for input side mosfet FDS86244 and optocoupler TCMT1107.

Could anyone please confirm if I can replace:

FDS86244 with SI1480DH [http://www.farnell.com/datasheets/1760640.pdf

or FDC8601 [http://www.farnell.com/datasheets/2000412.pdf]

or FDC3612 [http://www.farnell.com/datasheets/1639782.pdf]

Thank you for your assistance