Is it possible to achieve a circuit of Fig.2 of ucc2808 data seat?
The input voltage area which is 72V from 36V by Push - Pull system, can it correspond?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it possible to achieve a circuit of Fig.2 of ucc2808 data seat?
The input voltage area which is 72V from 36V by Push - Pull system, can it correspond?
Hi Kobayashi-san,
The push pull can be designed for this wide voltage range.
For example if the output duty cycle is 90% at 36V (corresponding to 45% duty cycle on each gate drive) then the required output duty cycle will be 45% at 72V
(corresponding to 22.5% duty cycle on each gate drive)
Does that make sense? Of course it is always difficult to design a power supply with a wide input range but it is possible to do so with the right care and attention to details
Regards,
John