I have questions about TPS54308 and TPS54202
Question 1. Output voltage Set Point
TPS54308 : datasheet p.15
TPS54202 : datasheet p.14
(In datasheet)
The 49.9-Ω resistor, R1, is provided as a convenient location to break the control loop for stability testing.
Must we use R1?
We want to reduce external parts.
Are there any concerns if we do not use R1.
Question 2. Feed-Forward Capacitor
TPS54202 : datasheet p.17
(In datasheet)
C6 is not needed when COUT has high ESR, and C6 calculated from Equation 16 should be reduced with medium ESR.
Please tell us the specific numerical value about high ESR and midium ESR.
What value is High ESR?
Whats value is midium ESR?
Question 3. Feed-Forward Capacitor
PS54308 and TPS5402
Must we use C6?
We want to reduce external parts.
We think C6 does not need if we use electrolytic capacitor in output capacitor.
Best regards,
Takahiro Nishizawa