Please note that E2E has undergone a major upgrade. Before logging in, please clear ALL your browser's cache and cookies.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54116-Q1: Adjusting the Output Voltage

Part Number: TPS54116-Q1

Could you please let me know in more details how to adjust the Output Voltage to 1.35 v given that the Vin is 3.3v?

Voltage Reference and Adjusting the Output Voltage
The voltage reference system produces a precise ±1% voltage reference over temperature by scaling the output

of a temperature stable bandgap circuit. The FB voltage is regulated to the voltage reference. The output voltage
is set with a resistor divider from the output node to the FB pin. It is recommended to use divider resistors with
1% tolerance or better. Start with a 10.0 kΩ for the bottom resistor RFBB and use the Equation 1 to calculate
RFBT. The maximum recommend resistance value for the bottom resistor is 100 kΩ.