Hi Expert,
I have some questions to the design example in datasheet 9.2.2 18-32Vin to 9Vpri and 12Viso following from below thread.
https://e2e.ti.com/support/power-management/f/196/t/808966?tisearch=e2e-sitesearch&keymatch=LM5160A
1. 12V is isolated output and 8V is primary output. So for primary output that cannot be no more than one half of the minimum input voltage is still a hard restriction or a just recommendation?
2. Is LM5160A good for customer's use case, 10-28Vin to 5.5Vpri and 15Viso? It looks it breaks the 50% duty rule however it can still run simulation on Webench. Please clarify.
Thanks.
Allan