Other Parts Discussed in Thread: BQ28Z610, BQSTUDIO, EV2400
Hi.
A Learning Cycle has been acquired in accordance with SLUA777.
Please answer the following questions.
1. The set value is determined according to SLUA777.
Please tell me how to reflect the setting value to another board
2. The following is described in SLUA777. Does this mean that the accuracy is reduced but the IT STATUS parameter can be operated without adjustment?
If the method does not require parameter adjustment, please provide details.
(The following content is excerpted from 4.2.1)
• An alternative method before starting this initial discharge would be to make sure impedance track is disabled.The GAUGE_EN flag of the manufacturing status register would be cleared if impedance track is disabled.If the GAUGE_EN flag is set, clear it by sending command 0x21 or clicking the GAUGE_EN button in the command window.This is different from earlier gauges in that IT enable command can be toggled on and off.In earlier gauges, once IT is enabled, it can never be disabled via command.Disabling impedance track prevents resistance updates from occurring during this initial discharge.
Hope to hear from you soon!