Other Parts Discussed in Thread: LM53603
Greetings,
I wanted to use MC33063A IC for bucking from 40V to 4V. The datasheet says "Switch Current Up to 1.5 A". My application would be to use this output to power up a few sensors, a microcontroller which combining would contribute to around 0.5A load. Along with that I would like to use SIM808 for Data Transmission which says "the peak current is nearly 2A for 577uS". The continuous current consumption of SIM808 is around 150mA.
Is it safe to use IC MC33063A for this application?
Thanks in advance