Hi,
I would like to ask you about TPS259541DSGR.
(question 1)
According to the 7.3 Recommended Operating Conditions section of the data sheet, I_LIM states that MAX 4A is the recommended value.
In addition, as a design guarantee value, it is stated that I_LIM can be used even at 5A at MAX.
Is it okay to set I_LIM between 4A and 5A?
(Question 2)
If I_LIM is set between 4A and 5A, the value of R_LIM may fall below the recommended value (MIN = 487Ω).
Is it okay to set it below 487Ω?
Is there a lower limit?
Best regards,