Hi,
Using version 1.3.104 of BQ Studio, I have initialized the BQ76952 (on a proprietary board) by writing the values on the Data Memory page (by Write_All after having imported my settings, see attached file).
After writing the DSG and CHG FETs are not activated, meaning I do not have a voltage on the Pack side. I tried applying a "charging voltage" on the pack side, which doesn't change anything. Electrically everything seems OK: cell voltages are reported correctle (I'm simulating 3 cells with a resistor network) and if I click on the "FET_ENABLE" command, the DSG FET is activated, resulting in a voltage on the Pack size. When I load the pack side with 2A, the CHG FET is activate as well, as expected. Charge/discharge current is then also reported correctly.
Looking at the registers (just after the data memory write, without any commands given in BQ Studio), I see that the XCHG and XDSG bits in the Alarm Raw Status register are set. But I don't understand why since none of the bits in the Safety and PR Alert registers are set as you can see in the snapshot below:
I would be very grateful if anyone can point out what I'm missing and what causes the FETS to remain off!
Thanks a lot for your time.
Jeroen
Attached you'll find the settings exported from the data memory page.
I also added the schematics, although I don't think the hardware is the problem.