I am using the TPS55288 with internal feedback set to the default ratio, which is fb_ratio = 0.0564
I have changed the REF value to be 10 0001 1101b (541 in decimal), which should set Vref = 655mV.
Given these two numbers, I believe the output voltage should be Vref/fb_ratio = 11.6V
However, I am seeing 15V on the output. Am I using the wrong equation? Thanks!