Hi,
I am currently doing some FOD calibration on a product and im trying to calculate the RPP package i receive from BQ51003 in order to enter it in the FOD calculation tool. In the qi specification the mention that you need to multiply the recieved value with the Maximum power, i copied the formula below.
Is the maximum power the one seen in the datasheet 2.5W? Or is it derived from the ILIM?
Lets say i receive the value 0x04 would the following then be the power in W that BQ51003 reports to the transmitter? P=(4/128)*2.5=78mW
BR Alexander