Other Parts Discussed in Thread: BQ25890
Hello,
Please Help!
I have a BQ24190 Evaluation board and am having trouble with the Narrow DC SYS output (Minimum System Voltage Regulation).
According to the data sheet, it should automatically regulate the SYS up to 3.5v (default) when the battery is below that value.
My output design has a 3v3 linear regulator that needs headroom so this feature is critical for me.
I cannot get the device to regulate the SYS to 3.5v (Minimum system voltage) no matter what registers I set or configuration I try.
Per the data sheet; I have a DC supply set to 3.2v and 2A on the BAT+ and GND terminals, I have also tried lower voltages down to 2.2v.
The SYS output ALWAYS follows the battery voltage, except when it is charging the battery, then it jumps up to 4.2v.
I can only get the device to go into "System Regulation" when the VBUS is connected to a USB device (charger) and the "OTG" is disabled.
Can you please advise a specific configuration to get the device to perform this on the Evaluation Board (bq24x9xEVM )?
I chose this chip because it seemed to be able to do this as a default, even independently without any Host commands.
Thank you in advance for your reply.