Other Parts Discussed in Thread: TPS7A90
Hi Team,
I am trying to find an IC with specs below:
Vin max >= 18V, Vout = 5V, Current >= 0.1A, accuracy = ± 1% (full temp range), the best package is SOT-89 (while other packages are also OK)
I only find one device TL780, while the accuracy is not ± 1% in full temp range, do you have some LDOs for recommendation?
THX a lot.