Hi,
I am trying to interface my Renesas MCU (R5F10PLJ) with TPS92662 over UART channels and trying to send a command to write the SYSCFG register during runtime but there is no response (Acknowledgement) from the TPS92662. Below are the details of the setup:
The MCU Baud rate configuration is set to 19,200 bps. MCU is also providing the clock to TPS92662 which is 19200 * 16 = 307.2kbps (as per datasheet the baud rate should be 16th of the clock). There is only one TPS 92662 on my board and I have set the ADDR0 pin to VDD, ADDR1 and ADDR2 to Gnd. The device ID is set as 0x61. The command that I am sending from MCU is
1. Write command to SYSCFG register -> {0x87, 0x61, 0x80, 0xA1, CRCL, CRCH} and then,
2. Read command to read the contents of SYSCFG register -> {0x99, 0x61, 0x80, CRCL, CRCH}
For both the commands there is no response from TPS. Also, I have tried loopback of the Tx and Rx channels of the MCU and it works, i.e., I am able to read send the bytes from the Tx channel and read it back on the MCU Rx channel and I am also getting the Rx and Tx interrupts in the MCU. But connecting it with TPS doesn't work. Please suggest any changes that would help in troubleshooting this issue.
Quick response will be really appreciated.
Thank you.
Sunil