Hello,
(1.) Regarding Figure 27 on P.30 of the TL431 spec, what is the recommended Vbat operating voltage range.
(2.) What is the recommended transistor in the same Figure. 27.
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
(1.) Regarding Figure 27 on P.30 of the TL431 spec, what is the recommended Vbat operating voltage range.
(2.) What is the recommended transistor in the same Figure. 27.
Thanks in advance.
Scott,
Vi Batt could be as low as 6V, if Rb is such that the TL431 cathode current is at least 1mA (not very practical, 7V or higher is easier).
In theory, there is no upper limit to Vi(batt), but TL431 cathode current must be less than 100mA and Rb rated for the power loss.
The transistor should be rated for the input voltage, output current, and power (Vi-Vo)*Iout. There is no output current limit other than VI(batt)/Rb*NPN beta.