https://e2e.ti.com:443/HI,We are using the TPS54821 device. Designed for 3.3V generation with 800KHz SW frequency. Suddenly we started to see a different behavior, when we probe the PH signal and Output signal after inductor, we are not seeing a constant voltage. Seeing a ramp up and down.We can see that from the attached waveform "3_3V_SWNode_Bad1". When we zoom the ramping area, we could see some switching happening, as shown in the waveform "3_3V_SWNode_Bad2".But on a good working board they are like the waveform "3_3V_SWNode_Good1".Kindly give some clarification behind the issue.Could be Inductor failure, MOSFET failure at the device, some auto frequency change (or) anything with Input voltage? We are seeing a constant 5V rails at the input.Regards,Felix.