Dear Experts,
I'm working with a case where TLV61220 is used for boosting 3.3V to 3.6V. Design needs to support battery as an alternative energy source. Battery is connected to TLV61220's output through diode.
When battery is used to power the design, TLV61220 is not used, meaning there is no input voltage and EN is low.
Is it harmful in any manner to connect voltage to TLV61220's output if part is not powered? When part is in that condition, is it possible to estimate the leakage current from battery to TLV61220's output?
Thanks!
Rgds,
Juha