Hi,
I am planning to use boost converter with following design parameters:
1) Input: 0.9 to 1.3 (I am using single Ni-MH cell)
2) Output: 3.3V fixed
3) Current requirement: >= 300mA
4) Package: which is easy to solder such as SOT-23, apart from WSON package
I am currently using TPS61021A, passive component for this IC have been calculated from TI webench application. It is taking good amount of passive components. If there any specific boost converter which gives fixed voltage of 3.3V with minimum number of passive.
Regards,
Tapas