Other Parts Discussed in Thread: LM5176
Hello,
Currently i have a working design using the LM5175 buck-boost controller.
The design works great and are currently in production. 20V-30V input, 24V 10A output.
The next project that i will be starting very soon is a system with very similar spec, only the output current will be increased to 20A (maybe higher).
According to the LM5175 product page, the maximum output current for this controller is rated to 20A.
I stop by this forum from time to time to do some browsing, and i have noticed over time that a 2-phase solution is recommended when outputting higher currents.
As i already have a working design made for 10A output, it would be great in terms of development time and time-to-market to reuse the design and put 2 circuits in parallell.
And therefore my question: Is it possible to use the LM5175 in such a parallell configuration? Maybe in a simular way as suggested in this app-note from Linear Technology?
If yes; is there any documentation available containing guidelines to do this with the LM5175?
If no; what other solutions can you suggest that i can use to meet my system requirements?
Best regards
-Mats