Other Parts Discussed in Thread: TPS61040, TPS61170
Hi,
I need to generate 100V,1mA typical from a 3.3V input supply.The power requirement is very low.There should not be any transformer in the design.
I was looking to low power dc-dc converters that could do the job.I came across parts like MAX15061,MAX15059,MAX15031which gives only upto 80V at output.
Is there any other similar solutions that can be help ful for me, ie something that provide 100V or above at boost output?
Or do you suggest using voltage multiplier configuration at the output from a lower voltage dc dc converter?
Thanks & Regards
Stephen Thomas