Do the sense pins have to be connected as close to the load as possible (it seems like the datasheet is suggesting it on page 2)? For example my Vout is 5V and the other side of my load is GND, can I just connect +sense to any +5V net and -sense through a via to my ground plane? Are there any special considerations I need to make during layout?