Other Parts Discussed in Thread: LMZ20502, TPS62130, TPS62135, TPS62136, LMZM33603, TPSM84824
Hi support,
I'm actually using a TPS82130 on my design to provide 2V5@1A max. from 12V. It gives me a Total Power Dissipation of 420mW max.
Thermal simulations show limitations because of power module reach approximatively 122°C in the worst case.
Datasheet specifies:
- A 10^5 hours lifetime for a Tj_max of 110°C.
- A 5*10^4 hours lifetime for a Tj_max of 125°C!
In comparison with the LMZ20502 (electrical caracteristics are not the same and it cannot be used in my application but package is a uSIP module as TPS82130):
I observe for LMZ20502, that thermal caracteristics seem better :
- Rjc_Top : 20.8°C/W
- RjC_Bot : 1.8°C/W
- Tjmax =125°C
For TPS82130:
- Rjc_Top : 9,4°C/W
- RjC_Bot : 21,3°C/W => It's pretty high for a QFN-like package? In comparison with LMZ205xx series.
- Tjmax =110°C (for better reliability)
What does it explain a such difference between these 2 components?
What is the expected lifetime for LMZ20502 at Tjmax=125°C?
What power module can I use to replace TPS82130 in my application? I'm initially searching for an uSIP component (can't find anyone) or any other regulator with a low footprint area and good thermal performance.
Thank you for your help.
Mickaël.