Part Number: AM623
Other Parts Discussed in Thread: TLV320AIC3101, TAS2780
Hi, TI expert!
I have a development environment for am6234, with our own evaluation board.
The evaluation board has a tlv320aic3101 audio codec chip.
The software SDK version is PROCESSOR-SDK-LINUX-RT-AM62X-08.06.00.42.
We attempted to use the mcasp of am6234 as the master device and the tlv320aic3101 codec chip as the slave device in I2S mode to record and playback a sound.
On the hardware side, we will connect a 12.288MHz crystal oscillator to the AUDIO_EXT_REFCLK1 pin, which will serve as an input and provide a clock signal of 12.288MHz to the AHCLKX of mcasp on am62x, as followings:
Now, for the software modifications, how should we modify the device tree and source code? Is there a detailed method for making these modifications?
Regards,
Li