Part Number: TDA4VM
Other Parts Discussed in Thread: DRA829,
Device: TDA4
SDK Vesion: sdk7_03
i have some problem for configured the sgmii
i read the Technical Reference Manual
<< J721E DRA829/TDA4VM Processors Silicon Revision 1.1 Texas Instruments Families of Products>>
5.1.3.4.62 CTRLMMR_SERDES1_LN0_CTRL Register ( Offset = 4090h) [reset = 0h]
| 1-0 | LANE_FUNC_SEL | R/W | 0h | Selects the SERDES1 lane0 function 0h - Enet Switch Q/SGMII Lane 3 1h - PCIe1 Lane 0 2h - For USB1 lane swap. Select this if USB1 was implemented with Type C connector 3h - ICSS_G1 SGMII Lane 0 |
5.1.3.4.63 CTRLMMR_SERDES1_LN1_CTRL Register ( Offset = 4094h) [reset = 0h]
| 1-0 | LANE_FUNC_SEL | R/W | 0h | Selects the SERDES1 lane1 function 0h - Enet Switch Q/SGMII Lane 4 1h - PCIe1 Lane 1 2h - USB1 3h - ICSS_G1 SGMII Lane 1 |
it look's like SERDES1 lane3 and lane4 can be used at the same time , but then i configured lane3 with