Part Number: TDA4VM
Hi,
If I've a camera sensor which output mipi csi signals in RGB888 format only, then how can I intruduce it's video into TDA4 EVM board and then goto DP port?
Since there is a description from this thread: RGB output from VISS is not recommended to be used, I have to do some work to figure the reasons out at least.
Here is what I understanding now, If I'm wrong please correct me.
The data path: Sensor(RGB888) --> Ser --> Des --> PDK.CSIRx --> FVID2 Driver --> TIOVX.Capture --> Multi/Single Cam App --> TIOVX.Display --> DP port --> Monitor.
The RGB888 support in each layers.

So, how many works need to be done to support RGB888? Or will it be supported in some version of PSDKR?
Thanks!