Part Number: TDA4VM
Hello,
I want to use the Single Camera Application on the J7 TDA4VM EVM.
I will use OnSemi AR0820 sensor as CSI input.
I want to do few changes of the application:
- I want that the VISS will output the video data as RGB888 instead of YUV420
- I want the output through DSS will be to DSI instead of eDP/HDMI
I need that the DSI will work at non-burst with sync pulses, and I need to disable the DCS command because I will connect the DSI stream to DSI analyzer and not to a display
What I need to do in order to implement the changes I want?
Thanks
Aharon Shpigel