This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: J7 TDA4VM EVM - Single Camera VPAC Application

Part Number: TDA4VM

Hello,

I want to use the Single Camera Application on the J7 TDA4VM EVM.

I will use OnSemi AR0820 sensor as CSI input.

I want to do few changes of the application:  

  1. I want that the VISS will output the video data as RGB888 instead of YUV420
  2. I want the output through DSS will be to DSI instead of eDP/HDMI

I need that the DSI will work at non-burst with sync pulses, and I need to disable the DCS command because I will connect the DSI stream to DSI analyzer and not to a display

What I need to do in order to implement the changes I want?

Thanks

Aharon Shpigel