This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello sir,
I'm Working on a custom EVMOMAPL138 board I was faced the issue in IP is not assigning in a custom board. I'm running the enet.echo source code from starter-ware packages. But it is working in development(LCDKOMAPL138) board and IP also assigned properly. We have cross-verified both side configurations (SW/HW) are fine. But for the development board, we have probed and checked the MDIO_CLK pin getting some pulse. But Custom board nothing it's coming but hardware side we had checked so many times still IP is not coming in EVMOMAPL138. If you know please let us inform.
Thanks in advance.
Regards
Seyed
Hi,
Can you be more specific on which IP you're working on so that I can assign this thread to the right expert?
Thanks,
Jianzhong
I have tried with both static and dynamic IP still I'm receiving 0.0.0.0 on a console. I'm using the example code of enet.echo in starter-ware packages.
Hi,
Which Process-SDK are you using, Linux or RTOS, and what's the version?
Thanks,
Jianzhong
Hi Seyed,
Sorry to mention that we don't have support for starterware anymore.
Thanks