Part Number: TI-CGT
Tools Setup for comparison:
Container (Ubuntu 16.04) : CCS10, T I5.2.9
Windows10 : CCS10, TI 5.2.9
Generation Mode : Using GUI
Container vs Windows Comparison :
-
When I am using following optimization settings , executable generated in both the platform are identical.
-Opt_level=off, --opt_for_speed=0ti -
When I select some other optimization settings (-Opt_level=1, --opt_for_speed=3), armcl is not generating identical executable.
Why compiler is not generating identical executable in both the platforms in 2 case ? Am I missing any specific compiler flag or setting ?