This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I want to know if USB0_DP/DM can be powered ahead of the power supply of AM3354. i have two chips communicated using USB, but the power of these two chips is from different power rail.
any risk for this connection?
thanks in advance!
Only USB0_VBUS and USB1_VBUS are fail-safe IO. The DP/DM signals are not and should not be driven before the AM335 has been powered.
See the Section 5.1 in the datasheet which identifies the fail-safe pins.
--Paul