This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Simultaneous Ethernet access from MCU Island and Main Island with Single PHY

Part Number: TDA4VM
Hello,
We would like to connect PHY to MCU Island in RGMII connection.
Is the Ethernet FW be capable of redirecting and allowing to use both the Ethernet traffic Main Island(A72) and MCU Island separately ?
The use case is as following :
1. Use only 1 PHY and connect to MCU Island
2. When in MCU Only mode to have the access to Ethernet still
3. When Main Island A72 is up, use for both Linux and MCU Island
4. Can Ethernet FW handle of sending both these traffic over single PHY?
Regards,
Kishore