Hi,
Blackhawk USB560v2 debugger is not getting detected in PC and also LED is not glowing from debugger as well.
Any help would be greatly appreciated.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Blackhawk USB560v2 debugger is not getting detected in PC and also LED is not glowing from debugger as well.
Any help would be greatly appreciated.
Hi Karan,
Two different version of debug adapter is there.
1st version which we are using for the current setup will support up to 12V.
2nd version of debug adapter will support up to 40V.
I was testing with 2nd version at 28V and then i have switched the debug adapter board to older version without changing the power supply to 12V.
It is not getting detected in other PC as well.
We are not seeing USB and MODE LED’s are blinking / glowing. Also, we are not detecting Blackhawk device on windows device manager and in CCS as well.
Regards,
Sankar
Hi Sankar, is this thread still open or were you able to work around this?
Regards
Karan