This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have the following issue when integrating SDK 7.03 onto RVP:
Basically I only managed to get camera streaming working for channel #0. It doesn't work for channel #1,#2, etc. I don't know if it is a sensor aliasing issue or something else. I noticed that the UDMA tied to these channels is not receiving the frame completion event, which caused the openVX capture node to wait forever..
Victor,
Can you please try single camera app with port #1?
Regards,
Mayank
Yes I tried that, port#1, port#2, port#3 but same result. Only port#0 works.